Other Parts Discussed in Thread: UCC29910, STRIKE, , UCC28070
I am trying to build a power factor correction converter for the following setup:
Line Voltage: 3 phase 400Vac (rectified Dc bus voltage is 540VDC).
Line input Voltage Range: 540VDC to 450VDC
Power: 5000W
Topology: PFC Buck using UCC29910
PFC output Voltage: 320VDC.
Is this setup possible to be realised with UCC29910 and complies with EN 61000-3-2.
The PFC Buck converter feeds a phase shift converter.(Input Voltage 320VDC,Output Voltage 10VDC, power: 5000W)
I aim to use semiconductors with lower Voltage rating. (600V instead, 1200V).
Second option may be to use a much lower PFC output Voltage such as 48VDC so that I can use semiconductors with much lower Voltage rating and much higher frequencies.(such as GaN)
The PFC Buck stage feeds a phase shift converter that is designed to deliver 10V @500A (5000W)
Any ideas or objections.