I have a BQ21040 charging IC connected as the data sheet describes. I am using a 10kohm resistor instead of the temperature sensor, the setting resistor is a 750ohm resistor and are expecting a quick charge current between 700 and 800 mA. The battery that is being charged is a 1200mAh 3.7v lithium polymer battery. So far we have been getting a constant current of around 105mA. Any help would be appreciated.