I have a 6s 22Ah battery. Achieved a successful learning cycle. Battery is designed for 125A continuous discharge.
Will attempt the scaling the current by following the instructions found in bq34z100-G1 High Cell Count and High Capacity Applications and in Gauge Design Configurations for High Charge / Discharge Rate Applications. Considering Ohm's law, I would think that the resistance values would be off by the same factor that the current is scaled by.
After following the instructions and changing the appropriate parameters, will the Ra tables now be invalid?