This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890H: possible to run auto detect without modifying registers

Part Number: BQ25890H


Is it possible to run the auto-detect without having it overwrite the input current limit register?

Thank you

  • Hi,

    No. In host mode, the host can force the device to run input current limit detection by setting FORCE_DPDM bit. After the detection is completed, FORCE_DPDM bit returns to 0 by itself and Input Result is updated.

    Thanks,

    Ning.
    Please click "This Resolved my issue" button if this post answer your question.