This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery Monitoring Solution.

Other Parts Discussed in Thread: BQ40Z50-R2, BQ40Z80

Sir,

We are looking for Battery Monitoring Solution

for 4 cell as well as 7 cell.

Parameters

Input Voltage 31.5 VDC  max

Over voltage detection:4.25 +/- 0.1V

Under voltage detection 2.5V  +/-0.3V

Over voltage & reverse polarity protection.

Cell balancing Range 70 - 90 mA

short circuit protection

Please suggest from the available solutions. 

Regards

Seema Joshi