This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: FLYBACK for +/-12V/10W

Part Number: TPS55340


Hello, customer is interested in the TPS55340 with Flyback topology. Can it be implemented with below conditions? or what else suggestions?

Input Voltage: 13V-18V

Output Voltage: +/-12V (Dual Output)

Output power: 10W

Is there similar ref. design with such conditions? 

application: EV Charging

Customer: WW  level 

Regards,

Brian W