Other Parts Discussed in Thread: BQ34110,
I am current using BQ34110 to monitor my IoT device battery on job site. There are multiple chemicals, such as, lead-acid and NiCd. I am also interested to replace it by BQ34210-Q1 on my design. My question is "Doese BQ34210-Q1 support single lead-acid battery?" The lead acid battery is not listed on the user manual (as below). I understand the voltage is up to 4.5V and my application is "single" lead-acid battery. Please let me know your comments. Thanks,
User Guide: The bq34210-Q1 fuel gauge incorporates gas gauging and an End-of-Service (EOS) Determination function to use with a 1-series Li-Ion or Lithium Iron Phosphate (LiFePO4) rechargeable cell or a Nickel metal hydride (NiMH) based pack with a configuration of 3-series cells.