This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C41-Q1: dc-dc

Part Number: UCC28C41-Q1
Other Parts Discussed in Thread: UCC2808A-2

lease help recommend the new DC/DC scheme, specific parameters requirements are as follows. Enter 9 x 35 V. Isolated output 12V / 5.5A 66W. Efficiency is no less than 90%. Operating temperature-30? 80.C.