Hi,
My customer is having two questions:
1. if TPS2546 can charging and transfer data at the same time in CDP mode?
If it's not CDP mode, what is the mode can support charging and data transfer at the same time?
2. they need 2.1 A for current limit, the fig39 show current goes up to 1.5A, will the current still follow BC1.2 protocol if setting the current limit to 2.1A?
Will it be climbing like the following capture?
Great thanks for your help.