Tool/software: WEBENCH® Design Tools
I have designed a 1000V,10W output flyback-SMPS with 12VDC input and frequency 1KHz using IC3843 and TI's Webench tool. I have calculated the transformer parameters using the IC datasheet and added the softstart functionality too. When I wired the components, the output voltage did not go beyond 200-300 V. However, when I remove the transistor connected to the ISENSE pin I get 1000V. I have added the DSO screenshot of the waveform observed at the ISENSE pin when the transistor is connected. How can I achieve 1000V with the transistor connected in the circuit?