Other Parts Discussed in Thread: UA78, TLV760, , UA78L
Hi,
these two LDO series seems identical at spec perspective.
Some customer is using L78L05ACD, should I recommend LM or UA?
Any general guideline when choosing between LM78 and UA78?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Howard,
Both of these devices should work for your application. The devices offer the same functionality and are available as a p2p replacement for the competition device.
Alternatively, if the customer can consider a different package I would recommend reviewing the TLV760 as a candidate to replace the competition device.
Howard,
TLV760 is the preferred option as it is an improved linear regulator which offers better dropout and IQ performance compared to the UA78L and LM78L devices.
Choosing between LM78L and UA78L boils downs to output option preferences as well as different package types. Both devices perform similarly and are available as a p2p option to the competition device.