Other Parts Discussed in Thread: UCC28070
UCC28063 datasheet states that it is suitable for up to 800W. What causes the limit, given that it is a controller?
Is there any other device to achieve 1000W?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Eddie,
The UCC28063 is a critical conduction mode PFC interleaved PFC pre-regulator. The peak currents are 2 times that of an average current mode control interleaved PFC pre-regulator. The RMS currents become more of an issue due to these peak current at output power ratings of more than 800W. For 800 W and above we recommended average current mode interleaved PFC using the UCC28070 interleaved PFC controller.
Regards,
Mike