Hi,
When using TPS27S100 RCP circuit as shown in datasheet figure 31, does the resistor need to withstand the full reverse polarity voltage (eg for a 1k Ohm resitor and 30V reverse voltage protection, I calculate the resistor needs to withstand a Pd of ~900mW)? Is that correct? The EVM uses a 0805 resistor with only 125mW and wondering if that will be sufficient?
Thanks & BR,
KF