Hey All,
So I've designed a circuit that uses the TPS54560 to switch a Variable Vin voltage source to and Ideal Vou of 24 volts. When the Vin is decreased to the point where Vout of 24V can no longer be achieved, Vout will also decrease linearly with the decrease of Vin. However when increasing the Vin back to a point such that Vout of 24V is possible (lets say Vin = 40V), the Vout appears to "latch" on the way back up and wont surpass approx 17V.
I've also tested this with the TPS54560-EVM board and get the same effect.
Any help would be greatly appreciated.
Cheers
Ricky