Other Parts Discussed in Thread: BQSTUDIO, EV2400
I am in the process of relaxing, discharging a battery pack to generate a golden file.
Here is my issue: The bqstudio is crashing after 6 or so hours when i am logging the data while the battery pack is relaxing.
I get 'Not able to find a free communications adapter' error and then data logging stops.
I have been told to relax the battery pack (LFP battery) for 5 to 10 hours. My next step is to discharge the battery at 200 mA and log the data. That would 22 hours of data logging.
I lose precious time whenever the crash happens.
What is causing the bqstudio to crash? i am using EVM2400.
What is the current draw of a EVM2400?
My setup has a laptop with EVM2400 connected to it and the EVM connected to my prototype which has the FG on it.
Please advise what could be causing this data crash on bqstudio?