Other Parts Discussed in Thread: TPS25940-Q1, TPS2595, TPS24750, TPS25982
Dear Sir/Ms.
The customer's purchaser request RD is looking for 2nd source to SY6875A.
Before we have recommended TPS25910 and TS25940-Q1 but the specifications are a little worse. Is there a better choice than TPS25910 and TPS25940-Q1?
Customer specifications are as follows
END Product is SSD.
1. Max. Vin > 20V
1, Current limit should be at least 3A or more (to be adjustable)
2, support 5V and 3.3V input at the same time
4, there is discharge (currently SY6875A also has no discharge function)
5, has clamping function
6, support -40~85 degrees
7, adjustable SS time (not necessary, better)
8, there is PG pin (not necessary, there is better)
Would you please give us some advice?
Best Regards,
Kami Huang