This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: UCC28070 GATE waveform issue

Part Number: UCC28070


Hello Tis

I use the UCC28070 in my 4000W AC/DC project, the input is 185Vac-264Vac, PFC output is 410V

but there are some waveform issues when the PFC output power is greater than 3000W, and causing the PFC MOS damage soon.

could you give me some advive, thx.

UCC28070 PFC design.rar