In regards to the values of the required capacitors and inductor, is there a range of values and/or equations to calculate values for this part?
Specifically:
- Can the bootstrap capacitor (SW to BTST) be any value other than 0.047uF? Like 1uF?
- Can the REGN capacitor (REGN to analog GND) be any value other than 4.7uF? Like 10uF?
- Can the VBUS capacitor be larger than 1uF? Like 10uF?
- Can the inductor be 4.7uH if sized properly according to 10.2.2.1 Inductor Selection in the datasheet and according to the following excerpt under 10.2.2.3?
The charger device has internal loop compensator. To get good loop stability, the resonant frequency of the
output inductor and output capacitor should be designed between 15 kHz and 36 kHz. The preferred ceramic
capacitor is 6 V or higher rating, X7R or X5R.