This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601RTWT

Other Parts Discussed in Thread: BQ25601, BQ2560, TPS22975

Hi,

There is an issue with the bq25601 on battery connection. We are using a single cell Li-Ion 3.7V battery connected to the BAT pin. The BATFET turns ON and the voltage appears on SYS pin but when it connects to the load the BATFET gets OFF and drops the voltage. However when I use the longer wire for my battery connector, it works fine. Wondering what is the issue?

  • Hi Habib,

    Can you give me some more information about your test setup? Are the battery and the load the only things connected to the board?

    If possible, a waveform showing VBAT, IBAT, VSYS, and ISYS when you connect the load for both cases (incorrect behavior and correct behavior with the longer wire) would be very helpful.

    Also, is the BATFET_DIS bit being set and latching the BATFET off?

    Best regards,
    Angelo
  • Hi Angelo,

    Here is the simplified block diagram: Looks like the BATFET of bq2560 tripping is due to the high inrush current. The rise time of the Load Switch is not high enough.

    Regards,

    Habib

  • Hi Habib,

    Your attachment isn't showing up for me.

    Based on your description though, it sounds like Section 8.3.2 of the datasheet. When you connect the load, the discharge current through the BATFET is too high, so the BQ25601 turns off the BATFET, causing your VSYS to drop. If the BATFET_DIS bit is being set, then that would confirm our suspicions.

    Best regards,
    Angelo
  • Hi Angelo, yes that is what happens and confirmed. Now we are looking at the best solution to prevent this from happening. Adding TPS22975 load switch with configurable rise time sounds is good solution. Any thought?
  • Hi Habib,

    I agree; adding a load switch with a configurable rise time sounds like a good solution to decrease the discharge current through the BATFET. Sections 10.2.2 and 10.2.3 of the TPS22975 datasheet discuss how to choose an appropriate capacitor value to limit inrush current. This application report may also be helpful to you: www.ti.com/.../slva670a.pdf

    Best regards,
    Angelo
  • Hi, Angelo,

    Thanks for your confirming this. However there is still one thing I'd like to get your thought on it. It is related to the section of 10.1.2 and 10.1.3 of the same data sheet on selecting the Cin and CL.

    Since our CL is too big (~2mF), I am wondering what would be the size of the Cin? the data sheet says it should be 10 times of the CL. Although the Cin is optional but CL can not be optional and it comes from my circuit's load capacitance. So how do you explain this? Do we really need such a big cap for Cin, in my case 20mF!!!

    Regards,

    Habib

  • Hi Habib,

    Sorry, I'm not sure about this because I only support battery charger ICs. Please create a new thread asking about the TPS22975 and the appropriate team within TI will get back to you.

    Best regards,
    Angelo