This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: Will this part work? Vin = 3.5V, Vout = 12V and I out = 0.4A?

Part Number: TPS61170
Other Parts Discussed in Thread: TPS61089, TPS61087, , TLV61046

Hi,

Please I need you help. The input is 3.5V and the output is 12V. When I simulate using webench it only allows me to go up to 0.2A. Does it mean it won't work when its 0.4A?

Thanks!