Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
I am using LM3481 for boost application,
syn pin to ground resistor is 200K ohm,
open loop test duty, max about 86%( spec= 85%),
but I try to add external clock = 150KHz (3V, duty=20%) signal at syn pin,
duty, max about 79%
Why is the duty,max going down?
thanks,
Burgess