This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53626: TPS53626RSMR

Part Number: TPS53626


Hi,

I want to get the full data sheet for the IC (part number: TPS53626RSMR) which we are planning to use in the solar charger application.

Our application requirement 

V_input = 0.58 V,    I_input = 0.8 A,    V_output = 5 V,  I_output = 50 mA to 100 mA.

Is this IC suitable for our application?

Regards,

John