Part Number: LP5912
Hello
I want to check If the pull_up voltage of PG could connect to other supply rather than Vout ? I 'm used LP5912-1.2, so If PG pull_up to Vout , the voltage on PG pin is 1.2V after IC start_up, and this 1.2V PGvoltage is too low for enable my second IC, so I want to pullup LP5912 PG pin to higher voltage such as LP5912's Vin_3.3V