Is it possible to distinguish between open-load and a short?
If yes can you explain me how?
Regards, Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to distinguish between open-load and a short?
If yes can you explain me how?
Regards, Bernd
Hello Bernd,
Do you mean short to ground or short to battery?
Hello Cameron,
I mean is it possible to distinguish between open-load and a short to ground?
Regards, Bernd
Can you confirm this possibility the customer found out:
Switching the input to low and the error comes again(as there is a 15k pull-up at the output) it was an OpenLoad else it was a short.
Does this work reliably?
Regards, Bernd
Bernd,
You are correct if you have an external pullup resistor and toggle input, if FAULT pin stays low then it is an open load. If it does not then it is a short.