Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5150-Q1: Input and output resistance of LM5150-Q1

Part Number: LM5150-Q1

Hi team,

Could you please kindly help on following questions?

#1 How much are the input and output resistance when the status of LM5150 is under shunt down mode ?  Though i can see some resistors from the block diagram(yellow masked), but i can't get these resistors' value. (customer want to evaluate the discharge time when there haven't Rload and the Vsupply changed from 6V(have stable Vout this time) to below 1V(shunt down mode))

#2 How long will it cost from EN enable to stable Vout (it is soft start time?)? I can't find relate parameter in Datasheet.

Thank you very much.

Best regards

Jessica