Hi Tiers.
When constant discharge current (about 250mA), SoC is correct working. (for example, SoC 10% at cell voltage 3.644V)
But when repeatedly discharging 150mA for 2 seconds and 15mA for 8 seconds, SoC is not correct at same cell voltage. (for example, SoC 20% at cell voltage 3.644V)
How can I fix it? Please help me.
I using Load Mode is 1.
At this fluctuating current discharge situation, What is right Load Mode?
And In Datasheet (6.3 Current/Power Profiles) it mentioned Load Mode 0 is default, But Table 16-3. In Data Flash Summary it mentioned Load Mode default value is 1.
Why different?