This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82084: TPS82084/85 maximum load capcitor

Part Number: TPS82084

Hello.

In the data sheet, there is a paragraph about output capacitor, which states "no more than 150uF"(page 11). Is that includes all the load capacitors? for example, if my load is a FPGA which requires a 330 uF capacitor- can I used this part?