This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2946: BQ294624 - Temperature limit behaviour

Part Number: BQ2946

Hello,

we have to check if the overvoltage detector  BQ294624 causes problems at overtemperature.

The data sheet shows +110 ° C and +85 ° C limits. 

We expect that it works up to +110°C.

We have a running series production.

If the limit is +85 ° C, that could be a problem.

What is the right operating temperature and what can happen if it reaches +105°C? 

Regards

Martin Hermann