Other Parts Discussed in Thread: BQ25505,
Hi,
insufficient input power
I want to know how can i avoid cold start .The following is the original data sheet. I want to know the detailed circuit diagram. appreciate!
我想要下面这段数据手册原文中的电路连接图,来避免冷启动,因为我的输入电压太低,vin_dc太低。感谢·感谢
The cold start circuit initially clamps VIN_DC to VIN(CS) = 600 mV typical. If sufficient input power (that is, output current from the harvester clamped to VIN(CS)) is not available, it is possible that the cold start circuit cannot raise the VSTOR voltage above VSTOR_CHGEN in order for the main boost conveter to start up. It is highly recommended to add an external PFET between the system load and VSTOR. An inverted VBAT_OK signal provided by VB_SEC_ON can be used to drive the gate of this system-isolating, external PFET.
My current circuit diagram(我现在还没加上面描述电路的初级电路图):