This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73606-Q1: LM73606-Q1: Feedback pin connection after sense resistor follow-up

Part Number: LM73606-Q1

Hello Frank,

After some simulations using the LM73606-Q1 spice model I have some follow-up question.

If the sense resistor is located immediately after the inductor it sees large current bursts which are problematic for accurate sensing and also for the sense resistor current limit.

Is it ok to have the following configuration:

Inductor -> decoupling capacitors -> sense resistors -> more decoupling capacitors -> load

Can I trust the LM73606-Q1 spice model to accurately represent waht I want to do?

Note: I must use the regulator in forced PWM

Thank you