Other Parts Discussed in Thread: PMP20497
Dear Sir/Ms.
My customers refer to the PMP20497 to design their products but now find the problems to trigger OCP.
www.ti.com/.../PMP20497
Customer specifications
Vin: 12V~56V
Vout: 55.5V/1A (system load 0A~0.6A)
The customer has sent us the PCB and circuit diagrams, and I can't touch the OCP with CT and R14. I see that the voltage of R12-R13 from the oscilloscope is 168mV.
Can you guide us how to adjust the parameters of OCP?
If you want customer's circuit diagram and other information, please email me. If you have a MathCAD (R14, R15) file, please email me.
Best Regards,
Kami Huang