Tool/software: Code Composer Studio
hello! everybody.
I have disigned an active balance system according ti_00817,connect to 14 Li-cell using two emb1428 and one emb1499.the cell is no. 0,1,2...13 according the posiiton of gnd.I find only no. 0,1,2,3 cell can do active balance.no.4,5,6...13 can not do active balance,the fault code is first 0b0001(primary current limit),after some seconds the fualt code is 0b1001(CS falling edge while slew is low or the EMB1428 is waiting for it to go high).I have work hard to resolve this problem.but I have no go well in three week.anyone can help me,why do the fault occur? thank you very much!