Hi,
I am looking for input high current protection fuse(Resettable) solution. below are the requirement details,
Input voltage : 24VDC/25A
Required Fuse Rating : 30VDC @ Ihold = ~26-27A, Itrip = 30A, These are minimum requirements.
Is there any working solution for the same or any other solution for high current protection?? Shall I go with two fuses in parallel??