This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
is there possibility to parallel LMG3410 to increase maximum current?
We are investigating possibility to use LMG3410R050 in our 3-level 3-phase current inverter but we have two options
- pure GaN transistors so we can do versions up to 240Amps (of transistor current -> 6mOhms)
- use LMG3410R050 but without parallel operation we are limited to 50mOhms resistance per transistor