This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: When selecting Ver.B

Part Number: LP8860-Q1


Hi All,

I chose Ver.B because it is 3.3V at a frequency of 300kHz.

But I do not use VSYNC.

In this case, is the LED lit if PWM is low ?

Best Regards,

Koji Hayashi