This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2543: Over-Current Protection w/o portable device

Part Number: TPS2543


Hi Team,

If portable device don't connect to TPS2543, Does Over-Current setting(based on CTL1-3, ILIM_SEL and ILIM_LO/HI setting) work well? or it will be 0.5A limitation?

Regards,

Kotaro Yamashita

  • Hello Kotaro,

    Yes, the overcurrent setting works when no device is connected to the TPS2543. Read through section 8.3.8 within the datasheet and this explains the two different scenarios where an over current event is triggered

    Hope this answers your question. If so, please click THIS RESOLVED MY ISSUE