Hi,
I have integrated the TPS63070 into my design, and the details are as follows
Vin= 3.5V(Li+ Battery)/Solar Power 3.5W/6V
Load= <200mA
Vout (Set):5.5V using Programmable resistors.
When i have fed the input voltage around 3.3V using the Li ion, to it, I cannot able to see the voltage at the output, after I started to Rise the Voltage to almost 4.0V then I can see the Output 5.5V at the Output terminals.
As per the specs from datasheet, it should be able to start feeding the output voltage at Input less than 2V,
what is the fix possibly that I have to do?