Other Parts Discussed in Thread: BQ24780S
Hi Team,
I am using the BQ24780SEVM for smart battery charge and discharge cycle. I have set the value 1% RSOC to charge the battery again,while discharging the battery at 1A discharge current the battery voltage reaches 12.4V and the RSOC is 3%.During this state the discharge current automatically goes to zero..
Used following below setting:
1) ChargeOption0 resistor value is 0x0108. while charging,
2) ChargeOption0 resistor value is 0x0129; while discharging.
Expecting Your reply at the earliest.
Regards,
Vel