This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27532-G1: Chem ID for Varta Battery for use with BQ27532

Part Number: BQ27532-G1

Hello,

I am using a battery from Varta, did a learning cycle and used the online chemid tool to get a chem ID. 

Not sure which Chem ID i should use?  or if I need to send in a sample of the battery to get a new chem Id profile.

Many thanks!

Sam

Chemistry ID selection tool, rev=2.42		
		
Configuration used in present fit:		
ProcessingType=2		
NumCellSeries=1		
ElapsedTimeColumn=2		
VoltageColumn=8		
CurrentColumn=14		
TemperatureColumn=7		
		
Best chemical ID : 455	Best chemical ID max. deviation, % : 4.02	
		
		
		
Summary of all IDs with max. DOD deviation below 15%		
		
Chem ID	max DOD error, %	Max R deviation, ratio
0	0	0
		
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
		
		
Selection of best generic ID for ROM based devices like bq274xx		
		
		
Device / Family #1		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27411-G1C: 4.35V LiCoO2	7.89
3142	bq27421-G1D: 4.4V LiCoO2	9.1
128	bq27421-G1A: 4.2V LiCoO2	34.18
312	bq27421-G1B: 4.3V LiCoO2	45.92
Best generic ID 354		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
Device / Family #2		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	7.89
1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	16.23
1202	bq27621: (default) 4.2V LiCoO2	20.38
Best generic ID 354		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
Device / Family #3		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
3230	bq27426: (default) 4.35V LiCoO2	7.89
3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	9.1
1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	20.38
Best generic ID 3230		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
Warning: Discharge rate is too high. High rate reduces ID detection accuracy	 10 hr rate is recomeended. Total discharge time is less than 5 hrs	 t_hrs=  4.64882