This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62745: Need a part similar to TPS62745

Part Number: TPS62745

Hi Team,

One of my customers is looking for a part similar to TPS62745 in features with only change being the selectable output voltage range.

In TPS62745, selectable output voltage range is 1.8-3.3V.

customer requirement for output voltage range is 2.5-4.0V. The output voltage needs to be selectable using VSEL pins with resolution of 0.1V.

 

Specifications:

  • Input Voltage Range VIN from 3.3 V to 10 V
  • Typical 400 nA Quiescent Current
  • Up to 90% efficiency with load currents >15 µA
  • Up to 300 mA Output Current
  • RF Friendly DCS-Control™
  • Low Output Ripple Voltage
  • 16 Selectable Output Voltages from
  • 2.5 V to 4.0 V
  • Integrated input voltage switch
  • Integrated Discharge Function at VOUT
  • Open Drain Power Good Output
  • Operates with a Tiny 3.3 µH or 4.7 µH Inductor
  • Small 3 mm × 2 mm WSON Package

Can you suggest the closest part which can meet these specifications?

Regards,

Harmeet