Hi team,
RTT values in the table 8 in the datasheet might be calculated by equation (3). It seems that the RTT value in 0.8V < Vout < 1.8 is almost consistent with the result from the eq (3). However, there are some gaps in 3.3V < Vout < 7.5V between RTT value in table 8 and calculated value by eq (3). I calculated the RTT value as the following table.
Could you check if the RTT values in table 8 is correct ?
| VOUT[V] | KTT | COUT1 Ceramic [uF] | COUT2 BULK[uF] | RTT[kΩ] | RTT Datasheet[kΩ] |
| 0.8 | 0.65 | 300 | 220 | 3.408 | 3.4 |
| 0.8 | 0.65 | 400 | 330 | 5.592 | 5.36 |
| 1 | 1 | 200 | 2 | 2 | |
| 1 | 0.6 | 200 | 220 | 3.04 | 3.01 |
| 1 | 1 | 400 | 6 | 6.04 | |
| 1 | 0.6 | 400 | 220 | 5.44 | 5.49 |
| 1.2 | 1.12 | 200 | 3.376 | 3.4 | |
| 1.2 | 0.6 | 200 | 220 | 4.048 | 4.02 |
| 1.2 | 1.12 | 400 | 8.752 | 8.87 | |
| 1.2 | 0.6 | 400 | 220 | 6.928 | 7.68 |
| 1.8 | 1.5 | 100 | 3.4 | 3.4 | |
| 1.8 | 1.5 | 300 | 14.2 | 14.3 | |
| 1.8 | 0.6 | 100 | 220 | 4.912 | 4.87 |
| 3.3 | 2 | 100 | 11.2 | 8.66 | |
| 3.3 | 0.9 | 100 | 220 | 17.008 | 31.6 |
| 3.3 | 2 | 200 | 24.4 | 19.1 | |
| 5 | 2 | 100 | 18 | 10 | |
| 5 | 1.2 | 100 | 220 | 36.4 | 31.6 |
| 5 | 2 | 200 | 38 | 22.1 | |
| 7.5 | 2.25 | 100 | 31.75 | 10.5 | |
| 7.5 | 1.8 | 47 | 220 | 70.09 | 28 |
Regards,
Saito