This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25896: STAT pin flashing at 12Hz

Part Number: BQ25896

Hi

I'm using the BQ25896 in its default state. No registers were altered. The STAT pin is flashing at 12Hz. The data sheet says it shall flash at 1Hz if there is a problem. If I unplug the battery, it does flash at 1Hz. As soon as I replace the battery, it starts flashing at 12Hz.  Why does it do this?

Thanks!