Hello E2E,
Our customer designed the 10-W transformer using UCC28740 calculation file.
Result, Lp=2600-uH, Rcs=1.8-ohm.
They said Lp and Rcs are too large. I have the same opinion.
At transformer for EVM, Lp=560-uH.
Does this calculation sheet calculate the correct result?
Customer's design spec;
Vin : DC220V to DC282V, Typ 260V
Vout : 5V
Iout : 2A
Regards,
ACGUY