This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2992: IC junction Temp

Part Number: LP2992


Hello Sir,

LP2992 Tj max is 125 degree C.

If our design is 12Vin and 3.3Vout  , 65mA

PD is 0.56W  so that refer to Theta JC is 122 for SOT23 package .

Will cause IC internal temp rising 69 degree C .  

System ambient Temp budget will only 125-69= 56 degree C max  <=  Am I right ?

Many thanks !

  • Hi Terry,

    It is important to understand that application specific conditions such as board layout, proximity to other heat sources, air flow, and ambient temperature will all impact the thermal performance of a linear regulator.  We model our Thermal Information table on the JEDEC Hi-K board.  This provides standardized layout and test configuration to compare the thermal characteristics of two packages and devices; however, your application specific conditions will impact the thermal performance in your application.

    Until you have a layout, the Rtheta_ja metric is useful in early calculations when trying to determine your ambient temperature budget:

    Tj = Pd x Rtheta_ja + Ta

    Tj = (Vin - Vout) x Iout x Rtheta_ja + Ta

    Your approach is correct to use the maximum operating temperature in order to calculate the maximum ambient temperature.

    125 C = 0.56 W x 169.7 C/W + Ta_max

    Ta_max = 125 C - 0.56 W x 169.7 C/W

    Ta_max = 30 C

    Please note that the WSON package has a much lower Rtheta_ja metric.  As such, you will be able to dissipate more power within the WSON package than the SOT-23 package.

    Very Respectfully,

    Ryan

  • Hello Ryan,

    Many thanks your support !
    May I know when/how to refer "ψJT" and "ψJB" . It is much lower than Theta parameters.
  • Hi Terry,

    We have several application notes which discuss how to use the thermal metrics located here.

    In particular, I believe the following two documents will be of interest for you:

     

     

    Very Respectfully,

    Ryan