Tool/software: Linux
Follow document ‘’bq33100 Super Capacitor Manager-Top 13 Design Considerations’’ item7 How to size the learning load?
- TI recommended that the learning current be high enough to provide at least a 25-mV drop, so ESR is 100 m ohm load current need 0.25A, but follow this example, I don’t know capacitor and load current relationship, why 2.5F capacitor need double load current?
- In our case, capacitor is 6.4F and ESR is 390 m ohm, I would like to calculation load current, please help to provide capacitor and load current relationship.
- If load current is too small, it will cause to learn process fail or time out (refer to the figure below).