This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: Compatible battery parameters

Part Number: BQ27510-G3

Information about compatible battery in datasheet and in this table is little bit different.
1) In datasheet there are no information about minimal battery capacity, but in the table it noted 300 mAh. So, why in table written 300 mAh? Will it work with my 250 mAh battery?

2) In datasheet everywhere written that device for Li-Ion batteries, but in one place (7.1 Overview) written: "The bq27510-G3 fuel gauge accurately predicts the battery capacity and other operational characteristics of a single Li-based rechargeable cell.", also in table written that Cell-cemistry is Li-Ion/Li-Polymer, so, what is actualy?

will this chip work with my Li-Po 250 mAh battery?