This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does someone know if a SOT23-5 LDO line regulator exists with its Vout on pin1?
I know its always on pin5 but maybe...
Hi Pascal,
While the more standard pin configuration for the SOT-23 package has OUT as pin 5, there are a few exceptions such as TPS709A.
When selecting an LDO it is important to know Vin, Vout, and Iout for the application. This information will help limit how many LDO datasheets you will need to look through to find your desired pinout.
Very Respectfully,
Ryan
Hello Ryan,
Thanks for your quick response!
The perfect linear reg for my retrofit 'quest' would be to replace the op amp in the circuit below with an linear reg of 2.5V without redesigning the PCB...
It has to be Vout=2.5V @30mA (min) and Vin=3.3V (but could be higher).
As you can see, Vout could be on pin 4. I can rotate the part if the pinout fits!