This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL1431-SP: TL1431-SP (5962R9962001VHA) NC pins

Part Number: TL1431-SP

Hello,

I'm using 5962R9962001VHA (Flatpack package) IC. However, the datasheet is confusing about NC pin connections. 1-) Do you have any SMD datasheet?

In page one, it is written that "NC-No Internal Connection". However, in page 2 anode is connected to 2,3,6,7 which are actually NC pins.

2-)Could you please provide me which NC pins aren't connected to anode, which NC pins are connected to anode for flatpack package?

3-)Also, could you please also correct that "real NC" defined pins are float?

Thank you.