Hello sir,
We have plan to use TPS65131 boost regulator in one our project
We need to design this regulator for following the specifications:-
Regulator input voltage = 5V
Regulator output voltage is ± 6 V with 700mA for both rails.
I will try generate this boost regulator circuit by using online TI Webbench design tool.
I can generate the circuit maximum 500mA at ±6V ouput rail.
But I can't generate circuit for 700mA at ±6V ouput rail . Tool showing error.
So please send us the TI webbench design PDF for >= 700mA at ±6V ouput rail.
Regards
Lakshmanan V