In the datasheet there in Table 5-5 there is a trigger event for SOC1 Set
In the low capacity section 5.4 it says there are 2 low capacity level flags named SOC1 and SOCCF. It states:
"The fuel gauge has two flags available in the Flags() register that warn when the SOC of the battery has
fallen to critically low levels."
I understand that I will get an interrupt when discharging and the state of charge goes below at the SOC1 threshold, but my question is will I get a separate (2nd) interrupt when the state of charge crossed the SOCF threshold?